Hardware requirements
Mini/micro USB cable
MIMXRT1060-EVKC board
Personal Computer
Board settings
Remove the resistor R305 and weld 0Ω resistor to R346,R350,R356,R362.
To make the example work, connections needed to be as follows:
SLAVE connect to MASTER
Pin Name Board Location Pin Name Board Location
SOUT J17-4 SIN SW2-3
SIN J17-5 SOUT SW2-2
SCK J17-6 SCK SW2-1
PCS0 J17-3 PCS0 SW2-4
Prepare the Demo
Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.
Open a serial terminal on PC for OpenSDA serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
You can see the similar message shows following in the terminal if the example runs successfully.
FLEXIO Master - LPSPI Slave polling example start.
This example use one flexio spi as master and one lpspi instance as slave on one board.
Master uses polling and slave uses interrupt way.
Please make sure you make the correct line connection. Basically, the connection is:
FLEXIO_SPI_master -- LPSPI_slave
CLK -- CLK
PCS -- PCS
SOUT -- SIN
SIN -- SOUT
This is LPSPI slave call back.
FLEXIO SPI master <-> LPSPI slave transfer all data matched!
End of example.