Hardware requirements
Micro USB cable
MIMX8MQ6-EVK board
J-Link Debug Probe
12V power supply
Personal Computer
Board settings
No special settings are required.
Please note this application can’t support running with Linux BSP!
Prepare the Demo
Connect 12V power supply and J-Link Debug Probe to the board, switch SW701 to power on the board
Connect a USB cable between the host PC and the J1701 USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Launch the debugger in your IDE to begin running the demo.
Running the demo
When the example runs successfully, you will find the LED RED is taking turns to shine.