Hardware requirements
Micro USB cable
MIMX8ULP-EVK/EVK9 Board
J-Link Debug Probe
5V power supply
Personal Computer
Board settings
No special is needed.
Prepare the Demo
Connect 5V power supply and J-Link Debug Probe to the board.
Connect a USB cable between the host PC and the Debug port on the board (Refer “MCUXpresso SDK Release Notes for EVK-MIMX8ULP and EVK9-MIMX8ULP.pdf” for debug port information).
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board (Please refer “MCUXpresso SDK Release Notes for EVK-MIMX8ULP and EVK9-MIMX8ULP.pdf” for how to run different targets).
Launch the debugger in your IDE to begin running the example.
Running the demo
When the example runs successfully, you can see the similar information from the terminal as below.
EDMA LPAV memory to memory transfer example begin.
Destination Buffer:
0 0 0 0
EDMA LPAV memory to memory transfer example finish.
Destination Buffer:
1 2 3 4