Hardware requirements
Micro USB cable
two MIMX8ULP-EVK/EVK9 board
JLink Plus
5V power supply
Personal Computer
Board settings
populate J8 for two boards. The example requires connecting between CAN pins of two boards. The connection should be set as follows:
Between two boards:
J8-1(CANH) node A, J8-1(CANH) node B
J8-2(CANL) node A, J8-2(CANL) node B
J8-3(GND) node A, J8-3(GND) node B
Prepare the Demo
Connect 5V power supply and JLink Plus to the board, switch SW10 to power on the board
Connect a micro USB cable between the host PC and the J17 USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the example runs successfully, following information can be seen on the terminal:
This message displays on the node A terminal:
********* FLEXCAN Interrupt EXAMPLE *********
Message format: Standard (11 bit id)
Message buffer 9 used for Rx.
Message buffer 8 used for Tx.
Interrupt Mode: Enabled
Operation Mode: TX and RX --> Normal
*********************************************
Please select local node as A or B:
Note: Node B should start first.
Node:a
Press any key to trigger one-shot transmission
Rx MB ID: 0x123, Rx MB data: 0x0, Time stamp: 8877
Press any key to trigger the next transmission!
Rx MB ID: 0x123, Rx MB data: 0x1, Time stamp: 32459
Press any key to trigger the next transmission!
This message displays on the node B terminal:
********* FLEXCAN Interrupt EXAMPLE *********
Message format: Standard (11 bit id)
Message buffer 9 used for Rx.
Message buffer 8 used for Tx.
Interrupt Mode: Enabled
Operation Mode: TX and RX --> Normal
Please select local node as A or B:
Note: Node B should start first.
Node:b
Start to Wait data from Node A
Rx MB ID: 0x321, Rx MB data: 0x0, Time stamp: 5759
Wait Node A to trigger the next transmission!
Rx MB ID: 0x321, Rx MB data: 0x1, Time stamp: 57276
Wait Node A to trigger the next transmission!