Hardware requirements
Micro USB cable
MIMX8ULP-EVK/EVK9 board
J-Link Debug Probe
5V power supply
Personal Computer
Board settings
No need special setting.
Please note this application can’t support running with Linux BSP!
Prepare the Demo
Connect 5V power supply and J-Link Debug Probe to the board, switch SW10 to power on the board.
Connect a micro USB cable between the host PC and the J17 USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download flash.bin for single boot type: a. Download to emmc(for single boot type) with uuu
uuu -b emmc imx-boot-imx8ulpevk-sd.bin-flash_singleboot_m33 flash.bin (Need download the file imx-boot-imx8ulpevk-sd.bin-flash_singleboot_m33 from linux bsp)
for low power boot type/dual boot type: a. Download to flexspi nor flash of m33 with uboot console(pls refer to the doc Getting Started with MCUXpresso SDK for EVK-MIMX8ULP and EVK9-MIMX8ULP.pdf) b. Download to flexspi nor flash of m33(for low power boot type/dual boot type) with jlink(pls refer to the doc Getting Started with MCUXpresso SDK for EVK-MIMX8ULP and EVK9-MIMX8ULP.pdf) c. Download to flexspi nor flash of m33 with uuu(write a uuu script to write flash.bin to flexspi nor flash of m33, pls refer to uuu manual)
Power Off board and Power on board
Note: Pls not running the demo that use TRDC with debugger(jlink or others)
Running the demo
When the example runs successfully, you can see the similar information from the terminal as below.
LPUART EDMA example
Send back received data
Echo every 8 characters