Hardware requirements

  • Mini/micro USB cable

  • EVK-MIMXRT1010 board

  • Personal Computer

Board settings

Remove the resistor R90 and weld 0Ω resistor to R800. To make the example work, connections needed to be as follows:

        SLAVE           connect to      MASTER
Pin Name   Board Location     Pin Name    Board Location
SOUT       J57-8                 SIN       J26-6
SIN        J57-10                SOUT      J26-4
SCK        J57-12                SCK       J26-8
PCS0       J57-6                 PCS0      J56-10

Prepare the Demo

  1. Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.

  2. Open a serial terminal on PC for OpenSDA serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

You can see the similar message shows following in the terminal if the example runs successfully.

FLEXIO Master - LPSPI Slave interrupt example start.

This example use one flexio spi as master and one lpspi instance as slave on one board.

Master and slave are both use interrupt way.

Please make sure you make the correct line connection. Basically, the connection is:

FLEXIO_SPI_master -- LPSPI_slave

      CLK        --    CLK

      PCS        --    PCS

      SOUT       --    SIN

      SIN        --    SOUT

This is LPSPI slave call back.

FLEXIO SPI master <-> LPSPI slave transfer all data matched!

End of example.

Note: To debug in qspiflash, following steps are needed:

  1. Select the flash target and compile.

  2. Set the SW8: 1 off 2 off 3 on 4 off, then power on the board and connect USB cable to J41.

  3. Start debugging in IDE.

    • Keil: Click “Download (F8)” to program the image to qspiflash first then clicking “Start/Stop Debug Session (Ctrl+F5)” to start debugging.