Hardware requirements

  • Mini/micro USB cable

  • Two EVK-MIMXRT1010 board

  • Personal Computer

Board settings

SPI two boards: Transfer data from one board instance to another board’s instance. SPI1 pins are connected with SPI1 pins of another board

       MASTER           connect to           SLAVE
Pin Name   Board Location     Pin Name    Board Location
SOUT       J57-10             SIN         J57-8
SIN        J57-8              SOUT        J57-10
SCK        J57-12             SCK         J57-12
PCS0       J57-6              PCS0        J57-6
GND        J57-14             GND         J57-14

Prepare the Demo

  1. Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.

  2. Open a serial terminal on PC for OpenSDA serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Reset the SoC and run the project.

Note: To debug in qspiflash, following steps are needed:

  1. Select the flash target and compile.

  2. Set the SW8: 1 off 2 off 3 on 4 off, then power on the board and connect USB cable to J41.

  3. Start debugging in IDE.

    • Keil: Click “Download (F8)” to program the image to qspiflash first then clicking “Start/Stop Debug Session (Ctrl+F5)” to start debugging.