Hardware requirements
Mini/micro USB cable
Two MIMXRT1024-EVK boards
Personal Computer
Board settings
To make the example work, connections needed to be as follows:
SLAVE connect to MASTER
Pin Name Board Location Pin Name Board Location
MOSI J18-12 MOSI J18-12
MISO J18-10 MISO J18-10
SCK J18-6 SCK J18-6
PCS0 J18-8 PCS0 J18-8
Prepare the Demo
Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.
Open a serial terminal on PC for OpenSDA serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
You can see the similar message shows following in the terminal if the example runs successfully.
FlexIO SPI interrupt example
Master Start...
Master runs successfully!
================================
Note: To debug in qspiflash, following steps are needed:
Select the flash target and compile.
Set the SW8: 1 off 2 off 3 on 4 off, then power on the board and connect USB cable to J23.
Start debugging in IDE.
Keil: Click “Download (F8)” to program the image to qspiflash first then clicking “Start/Stop Debug Session (Ctrl+F5)” to start debugging.