Hardware requirements
Mini/micro USB cable
EVK-MIMXRT595 board
Personal Computer
Board settings
To make the example work, connections needed to be as follows: Note: Please disconnect JS23 1-2, and connect JS23-2 to JP23-3 to provide 1.8V to VDDIO_3
SLAVE(SPI5) connect to MASTER(FlexIO0)
Pin Name Board Location Pin Name Board Location
MOSI JP26-2 MOSI J28-4
MISO JP26-3 MISO J28-5
SCK JP26-4 SCK J28-6
PCS0 JP26-1 PCS0 J28-3
Prepare the Demo
Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.
Open a serial terminal on PC for OpenSDA serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the demo runs successfully, the log would be seen on the terminal:
FLEXIO Master - SPI Slave interrupt example start.
This example use one flexio spi as master and one spi instance as slave on one board.
Master and slave are both use interrupt way.
Please make sure you make the correct line connection. Basically, the connection is:
FLEXI_SPI_master -- SPI_slave
SCK -- SCK
PCS0 -- PCS0
MOSI -- MOSI
MISO -- MISO
This is SPI slave call back.
FLEXIO SPI master <-> SPI slave transfer all data matched!