Hardware requirements
Micro USB cable
MIMXRT595-EVK board
Personal Computer
Board settings
Prepare the Demo
Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J40) on the board
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Launch the debugger in your IDE to begin running the demo.
Running the demo
The log below shows the output of the hello world demo in the terminal window:
FLEXSPI example started!
Vendor ID: 0xc2
Erasing Serial NOR over FlexSPI...
Erase data - successfully.
Program data - successfully.