Hardware requirements
Micro USB cable
EVK-MIMXRT595 board
Personal Computer
Board settings
Prepare the Demo
Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J40) on the board
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Launch the debugger in your IDE to begin running the demo.
Running the demo
When the example runs successfully, you can see the similar information from the terminal as below.
I2C example -- Read Accelerometer Value
Found an FXOS8700 on board , the device address is 0x1e .
The accel values:
status_reg = 0xff , x = 20 , y = -102 , z = 2102
status_reg = 0xff , x = 83 , y = -51 , z = 2089
status_reg = 0xff , x = 66 , y = -53 , z = 2101
status_reg = 0xff , x = 51 , y = -80 , z = 2098
status_reg = 0xff , x = 15 , y = -99 , z = 2105
status_reg = 0xff , x = 44 , y = -89 , z = 2097
status_reg = 0xff , x = 53 , y = -56 , z = 2099
status_reg = 0xff , x = 54 , y = -78 , z = 2103
status_reg = 0xff , x = 25 , y = -98 , z = 2098
status_reg = 0xff , x = 17 , y = -118 , z = 2107
End of I2C example .