Hardware requirements
Micro USB cable
EVK-MIMXRT595 REV C1 board
Personal Computer
Board settings
Make sure resistors R691~R697 are removed and resistors R611~R620,R660,R661,R698 are populated.
Prepare the Demo
Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J40) on the board
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Launch the debugger in your IDE to begin running the demo.
Running the demo
When the demo runs successfully, the log would be seen on the terminal like:
MMCCARD fatfs freertos example.
Make file system......The time may be long if the card capacity is big.
Create directory......
TASK1: write file successed.
TASK1: finished.
TASK2: write file successed.
TASK2: finished.
Note:This log is not constant, it depends on the SOC environment/software configuration, such as the SOC core clock, the task priority.