Hardware requirements

  • Micro USB cable

  • EVK-MIMXRT685 board

  • Personal Computer

Board settings

Prepare the Demo

  1. Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J5) on the board

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Launch the debugger in your IDE to begin running the demo.

Running the demo

The log below shows the output of the iap boot example in the terminal window and system will boot from the selected media:

===== IAP Boot example, input the parameter: =====
Boot mode (0: master, 1: ISP) : 0
Boot interface (0: USART 1: I2C 2: SPI 3: USB HID 4:FlexSPI 7:SD 8:MMC) : 4
Boot image index (0-1) : 0
Boot FlexSPI instance (0-3):
FlexSPI PortA1 = 0
FlexSPI PortB1 = 1
FlexSPI PortA2 = 2
FlexSPI PortB2 = 3
Selection : 1