Hardware requirements
Micro USB cable
EVK-MIMXRT685 board
Personal Computer
Board settings
No special settings are required.
Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J5) on the board
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Launch the debugger in your IDE to begin running the demo.
Running the demo
The log below shows example output of the SCTimer 16-bit counter demo in the terminal window:
SCTimer example to use it in 16-bit mode
The example shows both 16-bit counters running and toggling an output periodically
Probe oscilloscope at Q4-5(5Hz) and Q3-2(2.5Hz) to see output signal.