Hardware requirements

  • Mini/Micro USB cable

  • FRDM-K22F board

  • Personal Computer

Board settings

The example supports 2 different connections: Using 1 FRDM-K22F board: The 2 I2C instances on one board are used, one as I2C master , another as I2C slave. The connection should be set as following: - J24-12 , J1-13 connected - J24-10 , J2-07 connected Using 2 FRDM-K22F boards: The I2C0 module on one board is used as master. The I2C1 module on another board is used as slave. The connection should be se as following: - J24-12 (master board) connected to J1-13 (slave board). - J24-10 (master board) connected to J2-07 (slave board).

Prepare the Demo

  1. Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.

  2. Open a serial terminal on PC for OpenSDA serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. If using 1 FRDM-K22F board: Default settings in freertos_i2c.c is applied. Build project. Download the program to the target board. If using 2 FRDM-K22F boards: In file freertos_i2c.c in folder: boards\frdmk22f\rtos_examples\freertos_i2c, do following definition: #define EXAMPLE_CONNECT_I2C BOARD_TO_BOARD For master, use following definition #define I2C_MASTER_SLAVE isMASTER Build project. Download the program to one target board (used as master board). For slave, use following definition #define I2C_MASTER_SLAVE isSLAVE Build project. Download the program to one target board (used as slave board).

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the example runs successfully: If using 1 FRDM-K22F board, you can see the similar information from the terminal as below.

==FreeRTOS I2C example start.==

This example use one i2c instance as master and another as slave on one board.

Master will send data :

0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7

0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f

0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17

0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f

I2C slave transfer completed successfully.

Slave received data :

0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7

0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f

0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17

0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f

This time , slave will send data: :

0xff 0xfe 0xfd 0xfc 0xfb 0xfa 0xf9 0xf8

0xf7 0xf6 0xf5 0xf4 0xf3 0xf2 0xf1 0xf0

0xef 0xee 0xed 0xec 0xeb 0xea 0xe9 0xe8

0xe7 0xe6 0xe5 0xe4 0xe3 0xe2 0xe1 0xe0

Master received data :

0xff 0xfe 0xfd 0xfc 0xfb 0xfa 0xf9 0xf8

0xf7 0xf6 0xf5 0xf4 0xf3 0xf2 0xf1 0xf0

0xef 0xee 0xed 0xec 0xeb 0xea 0xe9 0xe8

0xe7 0xe6 0xe5 0xe4 0xe3 0xe2 0xe1 0xe0

End of FreeRTOS I2C example.

If using 2 FRDM-K22F boards, you can see the similar information from the terminal associated with master board and slave board as below.

For master:

==FreeRTOS I2C example start.==

This example use two boards to connect with one as master and another as slave.

Master will send data :

0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7

0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f

0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17

0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f

Master received data :

0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7

0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f

0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17

0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f

End of FreeRTOS I2C example.

For slave:

==FreeRTOS I2C example start.==

This example use two boards to connect with one as master and another as slave.

I2C slave transfer completed successfully.

Slave received data :

0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7

0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f

0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17

0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f

End of FreeRTOS I2C example.