Hardware requirements
Mini/micro USB cable
FRDM-K32L2A4S board
Personal Computer
USB To Serial Adapter
Board settings
Connect USB To Serial Adapter to user-defined pins, which are defined by “FLEXIO_UART_TX_PIN” and “FLEXIO_UART_RX_PIN” in source code. - PTE18, FLEXIO_UART_RX_PIN, J2-15 - PTE19, FLEXIO_UART_TX_PIN, J2-17 - GND , J2-14
Prepare the Demo
Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.
Open a serial terminal on PC for OpenSDA serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the demo runs successfully, the log would be seen on the terminal(from USB To Serial Adapter) like:
Flexio uart edma example
Board receives 8 characters then sends them out
Now please input: