Hardware requirements
Mini USB cable
FRDM-K32L3A6 board
Personal Computer
Board settings
To make the example work, connections needed to be as follows:
SLAVE(FXIO0) connect to MASTER(spi0)
Pin Name Board Location Pin Name Board Location
SOUT(PTE19,D9) J1 pin 7 SIN (PTC11) J4 pin 2
SIN (PTE13,D3) J1 pin 1 SOUT(PTC9) J2 pin 18
SCK (PTB15,D5) J3 pin 15 SCK (PTC30) J2 pin 13
PCS0(PTE21,D10) J1 pin 11 PCS0(PTC12) J4 pin 4
Prepare the Demo
Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.
Open a serial terminal on PC for OpenSDA serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
You can see the similar message shows following in the terminal if the example runs successfully.
FLEXIO Master - LPSPI Slave interrupt example start.
This example use one flexio spi as master and one lpspi instance as slave on one board.
Master and slave are both use interrupt way.
Please make sure you make the correct line connection. Basically, the connection is:
FLEXIO_SPI_master -- LPSPI_slave
CLK -- CLK
PCS -- PCS
SOUT -- SIN
SIN -- SOUT
This is LPSPI slave call back.
FLEXIO SPI master <-> LPSPI slave transfer all data matched!
End of example.