Hardware requirements
Mini/micro USB cable
FRDM-K32L3A6 board
Personal Computer
Board settings
This example project does not call for any special hardware configurations. Although not required, the recommendation is to leave the development board’s jumper settings and configurations in default state when running this example.
Prepare the demo
Connect a USB cable between the PC host and the OpenSDA USB port on the board.
Open a serial terminal on PC for OpenSDA serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Build core1 project first, then build core0 project.
Download the core0 program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the demo runs successfully, the log would be seen on the OpenSDA terminal like below and Red LED will turn on.
Sema42 example!
Press any key to unlock semaphore and Core 1 will turn off the LED
When press any key in the terminal, the LED will be turned off and the terminal tells
Now the LED should be turned off
Sema42 example succeed!