Hardware requirements
Micro USB cable
FRDM-KE15Z board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the example runs successfully, the following message is displayed in the terminal:
LPI2C example -- Read Accelerometer Value
Found a FXOS8700 on board , the device address is 0x1C .
The accel values:
status_reg = 0xff , x = 60 , y = -80 , z = 2094
status_reg = 0xff , x = 54 , y = -73 , z = 2088
status_reg = 0xff , x = 54 , y = -77 , z = 2096
status_reg = 0xff , x = 57 , y = -79 , z = 2096
status_reg = 0xff , x = 57 , y = -83 , z = 2089
status_reg = 0xff , x = 55 , y = -78 , z = 2102
status_reg = 0xff , x = 56 , y = -77 , z = 2097
status_reg = 0xff , x = 57 , y = -77 , z = 2085
status_reg = 0xff , x = 59 , y = -78 , z = 2094
status_reg = 0xff , x = 56 , y = -79 , z = 2093
End of LPI2C example .