Hardware requirements
Micro USB cable
FRDM-KE17Z board
Personal Computer
Board settings
The example requires connecting the FLEXIO pins with the LPSPI pins The connection should be set as following: MASTER connect to SLAVE Pin Name Board Location Pin Name Board Location SOUT J2 pin 15 SIN J2 pin 10 SIN J1 pin 7 SOUT J2 pin 8 SCK J2 pin 17 SCK J2 pin 12 PCS J1 pin 5 PCS1 J2 pin 6
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the example runs successfully, the following message is displayed in the terminal:
FLEXIO Master - LPSPI Slave interrupt example start.
This example use one flexio spi as master and one lpspi instance as slave on one board.
Master and slave are both use interrupt way.
Please make sure you make the correct line connection. Basically, the connection is:
FLEXI_SPI_master -- LPSPI_slave
CLK -- CLK
PCS -- PCS
SOUT -- SIN
SIN -- SOUT
This is LPSPI slave call back.
FLEXIO SPI master <-> LPSPI slave transfer all data matched!
End of example.