Hardware requirements
Type-C USB cable
FRDM-MCXA153 board
Personal Computer
Board settings
Prepare the Demo
Connect a Type-C USB cable between the host PC and the MCU-Link port(J15) on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Press reset button to begin running the demo.
Running the demo
The log below shows the output of the hello world demo in the terminal window:
I3C master read sensor data example.
Temperature:27.000000
Temperature:27.000000
......