Hardware requirements
Type-C USB cable
FRDM-MCXA153 board
Personal Computer
Board settings
Pin Name Board Location checker channel number pre-set value trigger
P2_2 J2-9 channel 0 1 input > DAC output
P1_3 J6-3 channel 1 0 input < DAC output
P1_4 J1-2 channel 2 1 input > DAC output
This example uses LPCMP0 instance, the fixed port is plusMuxPort, the fixed channel is channel 7(Internal DAC module), and the checker channels are channel 0(CMP0_IN0, P2_2, J2-9), channel 1(CMP0_IN1, P1_3, J6-3) and channel 2(CMP0_IN2, P1_4, J1-2), in miusMuxPort. The LPCMP’s internal DAC module output voltage signal(half of VREFI), the channel’s pre-set value is 0x05U.
Set the input voltage of channel 0, channel 1 and channel 2 to be greater than, less than and greater than the output voltage of the DAC respectively. The comparison results of the three channels are different from the pre-set value. So the interrupt occurred and the terminal will print corresponding channel changed information.
Prepare the Demo
Connect a Type-C USB cable between the host PC and the MCU-Link port(J15) on the target board.
Open a serial terminal on PC for the serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the demo runs successfully, following information can be seen on the OpenSDA terminal:
LPCMP RoundRobin Example.
channel 0 comparison result is different from preset value!
channel 1 comparison result is different from preset value!
channel 2 comparison result is different from preset value!