Hardware requirements
USB-C cable
Loopback network cable RJ45 standard
FRDM-MCXE247 board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a USB cable between the host PC and the MCU-LINK USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Insert loopback network cable to Ethernet RJ45 port.
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Make loopback network cable:
568B standard Unknown standard
J1 orange+white green+white
J2 orange green
J3 green+white orange+white
J4 blue brown+white
J5 blue+white brown
J6 green orange
J7 brown+white blue
J8 brown blue+white
Connect J1 => J3, J2 => J6, J4 => J7, J5 => J8. 10/100M transfer only requires J1, J2, J3, J6, and 1G transfer requires all 8 pins. Check your net cable color order and refer to 568B standard or the other standard. If your cable’s color order is not shown in the list, please connect J1~J8 based on your situation.
Running the demo
When the demo runs, the log would be seen on the terminal like:
ENET example start.
Wait for PHY init...
Wait for PHY link up...
The 1 frame transmitted success!
A total of 1 frame(s) has been successfully received!
The 2 frame transmitted success!
A total of 2 frame(s) has been successfully received!
The 3 frame transmitted success!
A total of 3 frame(s) has been successfully received!
......
The 20 frame transmitted success!
A total of 20 frame(s) has been successfully received!