Hardware requirements
Type-C USB cable
FRDM-MCXN236 board
Personal Computer
Board settings
P4_19(J8-11) connect to CTimer simple PWM.
Prepare the Demo
Connect a type-c USB cable between the PC host and the MCU-Link USB port (J10) on the board
Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The log below shows example output of the CTimer simple PWM demo using interrupts in the terminal window:
CTimer example to generate a PWM signal
This example uses interrupts to update the PWM duty cycle