Hardware requirements
Type-C USB cable
FRDM-MCXN947 Board
Personal Computer
Board settings
To make the example work, connections needed to be as follows:
MASTER(FlexIO SPI) connect to SLAVE(FlexIO SPI)
Pin Name Board Location Pin Name Board Location
SOUT J8 pin 26 SIN J8 pin 26
SIN J8 pin 25 SOUT J8 pin 25
SCK J8 pin 27 SCK J8 pin 27
PCS0 J8 pin 28 PCS0 J8 pin 28
Prepare the Demo
Connect a USB cable between the host PC and the EVK board J17.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The log below shows the output of the hello world demo in the terminal window:
FlexIO SPI interrupt example
Slave is working...
Slave runs successfully!