Hardware requirements

  • Mini/micro USB cable

  • FRDM-MCXN947 board

  • Personal Computer

Board settings

Jumper settings for OM- SE050ARD & OM- SE051ARD: -J14 3-4 (Default): EdgeLock SE05x_VCC pin routed to SE05X_VOUT pin -J15 3-4 (Default): I2C target SDA connection -J17 3-4 (Default): I2C target SCL connection

For A71CH

  • Connect OM3710/A71CHARD to the board.

For SE050

  • Connect OM- SE050ARD to the board.

  • Please consult SE050 user manual and Plug & Trust middleware documentation which is present in the Plug & Trust MW package for further details.

  • The Plug & Trust MW package can be downloaded from https://www.nxp.com/products/security-and-authentication/authentication/:SE050?tab=Design_Tools_Tab

  • Please refer to the RST file in the doc folder for additional details about the example.

  • For running ex_rsa example enable following options in the fsl_sss_ftr.h file: SSS_HAVE_APPLET_SE05X_C - 1 SSS_HAVE_RSA - 1