Overview

This document provides step-by-step procedures to build and test coex examples, and also instructions for running the included sample applications.

Hardware requirements

  • Type-C cable

  • FRDMRW612 board

  • Personal Computer

Board settings

No specail setting to do for wifi&ble coex.

Build and flash

Building

Modify examples/coex_examples/coex_wifi_edgefast/app_config.cmake to generate different coexistence images.

coexistence images

CONFIG_WIFI

CONFIG_BLE

WiFi + BLE

1

1

Macors releated to Wi-Fi supplicant

Wi-Fi supplicant

CONFIG_WPA_SUPPLICANT

embedded supplicant

0

wpa supplicant

1(default)

Enable Monolithic feature

Modify examples/${board}/coex_examples/coex_wifi_edgefast/app_config.h.

Component

CONFIG_MONOLITHIC_WIFI

CONFIG_MONOLITHIC_BLE

CONFIG_MONOLITHIC_BLE_15_4

Wi-Fi

1(default)

NA

NA

BLE

NA

1(default)

NA

If want to disable Wi-Fi monolithic feature, define CONFIG_MONOLITHIC_WIFI to 0. If want to disable BLE monolithic feature, define CONFIG_MONOLITHIC_BLE to 0.

Building coex examples

flash_debug:

$ cd <sdk root>
$ west build -b frdmrw612 examples/coex_examples/coex_wifi_edgefast --toolchain armgcc --config=flash_debug -d coex_wifi_edgefast

flash_release

$ cd <sdk root>
$ west build -b frdmrw612 examples/coex_examples/coex_wifi_edgefast --toolchain armgcc --config=flash_release -d coex_wifi_edgefast

NOTE:

  1. -d coex_wifi_edgefast -> Specify the generated project path. Can name it as needed.

  2. Find coex_wifi_edgefast.elf/coex_wifi_edgefast.bin in coex_wifi_edgefast folder.

  3. Only support armgcc to build coex application.

Flash Binaries

Flash the image with the following command,

# CMD to write CPU3 coex app image to flash in J-link window:
J-Link> loadbin C:\xxx\coex_wifi_edgefast.bin, 0x08000000

NOTE:

Monolithic feature is default enabled, this means it’s no need to flash binaries manually.

If disable Wi-Fi or BLE monolithic feature, download firmware manually.

SB firmware path: mcu-sdk-3.0/components/conn_fwloader/fw_bin

# CMD to write CPU1 wifi image to flash in J-link window:
J-Link> loadbin C:\xxx\rw61x_sb_wifi_a2.bin,0x08400000
# CMD to write CPU2 ble to flash in J-link window:
J-Link> loadbin C:\xxx\rw61x_sb_ble_a2.bin,0x08540000

Run

Prepare the Demo

  1. Connect a micro USB cable between the PC host and the MCU-Link USB port (J7) on the board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Launch the debugger in your IDE to begin running the example.

Running the example

The log below shows the output of the coex examples (based on edgefast-shell) in the terminal window:

        Coex APP

SHELL build: ========================================
========================================
     Initialize RW612 Module
========================================
May 14 2024
Copyright  2020  NXP
========================================

WiFi shell initialization
========================================
BLE shell initialization
@bt> ========================================

@Coex>
  1. WiFi Test

NOTE: All wifi commands require adding wifi. prefix.

  • Get the Wi-Fi driver and firmware version:

@Coex> wifi.wlan-version
WLAN Driver Version   : v1.3.r48.p10
@Coex> WLAN Firmware Version : rw610w-V2, IMU, FP99, 18.99.6.p6, PVE_FIX 1
Command wlan-version
  • Get MAC Address:

@Coex> wifi.wlan-mac
MAC address
@Coex> STA MAC Address: 00:50:43:02:98:23
uAP MAC Address: 00:50:43:02:99:23
Command wlan-mac
  • Scan the network:

@Coex> wifi.wlan-scan
Scan scheduled...
@Coex> Command wlan-scan
2 networks found:
1C:6A:7A:87:FF:BF  "NXP" Infra
        mode: 802.11AC
        channel: 161
        rssi: -74 dBm
        security: WPA2 Enterprise
        WMM: YES
        802.11K: YES
        802.11V: YES
        802.11W: NA
        WPS: NO
1C:6A:7A:87:FF:BE  "NXPOPEN" Infra
        mode: 802.11AC
        channel: 161
        rssi: -75 dBm
        security: WPA2
        WMM: YES
        802.11K: YES
        802.11V: YES
        802.11W: NA
        WPS: NO
  1. BLE Test

NOTE: Please use the command “help” to view the specific commands supported by the example.

  • BLE scan devices (the BLE host must initialized before):

@Coex> bt.init
@Coex> Bluetooth initialized
Settings Loaded

@Coex> bt.scan on
Bluetooth active scan enabled
@Coex> [DEVICE]: 44:6D:F5:85:DC:5F (random), AD evt type 0, RSSI -64  C:1 S:1 D:0 SR:0 E:0 Prim: LE 1M, Secn: No packets, Interval: 0x0000 (0 ms), SID: 0xff
[DEVICE]: 44:6D:F5:85:DC:5F (random), AD evt type 4, RSSI -63  C:0 S:1 D:0 SR:1 E:0 Prim: LE 1M, Secn: No packets, Interval: 0x0000 (0 ms), SID: 0xff
[DEVICE]: 6D:B3:D3:8E:ED:A2 (random), AD evt type 0, RSSI -77  C:1 S:1 D:0 SR:0 E:0 Prim: LE 1M, Secn: No packets, Interval: 0x0000 (0 ms), SID: 0xff
[DEVICE]: 6D:B3:D3:8E:ED:A2 (random), AD evt type 4, RSSI -76  C:0 S:1 D:0 SR:1 E:0 Prim: LE 1M, Secn: No packets, Interval: 0x0000 (0 ms), SID: 0xff
[DEVICE]: 3F:FB:95:F7:F9:14 (random), AD evt type 3, RSSI -75  C:0 S:0 D:0 SR:0 E:0 Prim: LE 1M, Secn: No packets, Interval: 0x0000 (0 ms), SID: 0xff
[DEVICE]: 49:A3:4E:86:63:0C (random), AD evt type 0, RSSI -76  C:1 S:1 D:0 SR:0 E:0 Prim: LE 1M, Secn: No packets, Interval: 0x0000 (0 ms), SID: 0xff
[DEVICE]: 49:A3:4E:86:63:0C (random), AD evt type 4, RSSI -75  C:0 S:1 D:0 SR:1 E:0 Prim: LE 1M, Secn: No packets, Interval: 0x0000 (0 ms), SID: 0xff
[DEVICE]: 5C:28:50:F9:DD:57 (random), AD evt type 0, RSSI -82  C:1 S:1 D:0 SR:0 E:0 Prim: LE 1M, Secn: No packets, Interval: 0x0000 (0 ms), SID: 0xff
[DEVICE]: 4A:7D:B4:12:7B:7A (random), AD evt type 0, RSSI -82  C:1 S:1 D:0 SR:0 E:0 Prim: LE 1M, Secn: No packets, Interval: 0x0000 (0 ms), SID: 0xff
[DEVICE]: 4A:7D:B4:12:7B:7A (random), AD evt type 4, RSSI -82  C:0 S:1 D:0 SR:1 E:0 Prim: LE 1M, Secn: No packets, Interval: 0x0000 (0 ms), SID: 0xff
[DEVICE]: 5A:54:C8:99:13:4A (random), AD evt type 0, RSSI -76  C:1 S:1 D:0 SR:0 E:0 Prim: LE 1M, Secn: No packets, Interval: 0x0000 (0 ms), SID: 0xff
[DEVICE]: 3B:95:00:4D:F3:EB (random), AD evt type 3, RSSI -82  C:0 S:0 D:0 SR:0 E:0 Prim: LE 1M, Secn: No packets, Interval: 0x0000 (0 ms), SID: 0xff
[DEVICE]: 47:9D:D0:CB:5F:0D (random), AD evt type 0, RSSI -86  C:1 S:1 D:0 SR:0 E:0 Prim: LE 1M, Secn: No packets, Interval: 0x0000 (0 ms), SID: 0xff
@Coex> bt.scan off
Scan successfully stopped
@Coex>
  • BLE advertise (the BLE host must initialized before):

@Coex> bt.init
@Coex> Bluetooth initialized
@Coex> bt.advertise on
Advertising started
@Coex> bt.advertise off
Advertising stopped
  • BLE connect (the BLE host must initialized before):

@Coex> bt.init
@Coex> Bluetooth initialized
@Coex> bt.connect C0:95:63:23:55:87 random
Connection pending
Connected: 7D:FD:FD:4D:FD:90 (random)
  • BLE pairing and bonding:

GATT peripheral role side,
1. Initialize the Host, press "bt.init",
2. Advertising, press "bt.advertise on",
3. After the connection is established, perform the pairing sequence,
   it could be started from peripheral side by pressing "bt.security <level>", such as "bt.security 2".
4. If the bondable is unsupported by peripheral role, press "bt.bondable off". Then start step 3.

GATT central role side,
1. Initialize the Host, press "bt.init",
2. Scaning advertising packets, press "bt.scan on",
3. A few seconds later, stop the scanning, press "bt.scan off"
4. Select the target board and create a new connection. If the taregt is not listed, repeat steps 2 and 3.
   Then press "bt.connect <address: XX:XX:XX:XX:XX:XX> <type: (public|random)>"
5. After the connection is established, perform the pairing sequence,
   it could be started from central side by pressing "bt.security <level>", such as "bt.security 2".
6. If the bondable is unsupported by central role, press "bt.bondable off". Then start step 5.
  • BLE 1M/2M/Coded PHY update:

GATT peripheral role side,
1. Initialize the Host, press "bt.init",
2. Advertising, press "bt.advertise on",
3. After the connection is established.
4. Send phy update command, press "bt.phy-update <tx_phy> [rx_phy] [s2] [s8]", tx_phy/rx_phy could be 1(1M) or 2(2M) or 4(Coded).
   such as "bt.phy-update 2 2".
5. The message "LE PHY updated: TX PHY LE 2M, RX PHY LE 2M" would be printed if the phy is updated. note, if peer do not support phy update, then this message will not be printed.

GATT central role side,
1. Initialize the Host, press "bt.init",
2. start scan, press "bt.scan on", Bluetooth device around your current bluetooth will be list, for example,
[DEVICE]: 72:78:C1:B5:0F:DA (random), AD evt type 4, RSSI -32 BLE Peripheral C:0 S:1 D:0 SR:1 E:0 Prim: LE 1M, Secn: No packets, Interval: 0x0000 (0 ms), SID: 0xff
[DEVICE]: C4:0D:02:55:5E:AD (random), AD evt type 0, RSSI -83  C:1 S:1 D:0 SR:0 E:0 Prim: LE 1M, Secn: No packets, Interval: 0x0000 (0 ms), SID: 0xff
[DEVICE]: 66:8F:26:27:1F:52 (random), AD evt type 0, RSSI -82  C:1 S:1 D:0 SR:0 E:0 Prim: LE 1M, Secn: No packets, Interval: 0x0000 (0 ms), SID: 0xff
3. stop scan, press "bt.scan off",
4. connect target device, press "bt.connect <address: XX:XX:XX:XX:XX:XX> <type: (public|random)>", such as bt.connect 72:78:C1:B5:0F:DA random
5. Send phy update command, press "bt.phy-update <tx_phy> [rx_phy] [s2] [s8]", tx_phy/rx_phy could be 1(1M) or 2(2M) or 4(Coded).
   such as "bt.phy-update 2 2".
6. The message "LE PHY updated: TX PHY LE 2M, RX PHY LE 2M" would be printed if the phy is updated. note, if peer do not support phy update, then this message will not be printed.
  • BLE Data Packet Length Extension update:

GATT peripheral role side,
1. Initialize the Host, press "bt.init".
2. Advertising, press "bt.advertise on".
3. After the connection is established.
4. Check current LE RX/TX maximum data length and time, press "bt.info", as blow, default RX/TX maximum data length is 27 and default RX/TX maxumum time is 328.
Type: LE, Role: slave, Id: 0
59:8F:3C:20:93:86 (random)
Remote address: 59:8F:3C:20:93:86 (random) (resolvable)
Local address: 80:D2:1D:E8:30:EC (public) (identity)
Remote on-air address: 59:8F:3C:20:93:86 (random) (resolvable)
Local on-air address: 7C:59:48:2E:A4:51 (random) (resolvable)
Interval: 0x0024 (45 ms)
Latency: 0x0000 (0 ms)
Supervision timeout: 0x0190 (4000 ms)
LE PHY: TX PHY LE 1M, RX PHY LE 1M
LE data len: TX (len: 27 time: 328) RX (len: 27 time: 328)
5. When LE data len is updated by the peer device, below information will be printed.
LE data len updated: TX (len: 27 time: 328) RX (len: 50 time: 512)
6. Update maximum tx data length, press "bt.data-len-update <tx_max_len> [tx_max_time]", such as bt.data-len-update 65, below information will be printed.
Calculated tx time: 632
59:8F:3C:20:93:86 (random)
data len update initiated.
LE data len updated: TX (len: 65 time: 632) RX (len: 50 time: 512)

GATT central role side,
1. Initialize the Host, press "bt.init".
2. Start scan, press "bt.scan on", Bluetooth device around your current bluetooth will be list, for example, 
[DEVICE]: 7C:59:48:2E:A4:51 (random), AD evt type 4, RSSI -44 BLE Peripheral C:0 S:1 D:0 SR:1 E:0 Prim: LE 1M, Secn: No packets, Interval: 0x0000 (0 ms), SID: 0xff
3. Stop scan, press "bt.scan off",
4. Connect target device, press "bt.connect <address: XX:XX:XX:XX:XX:XX> <type: (public|random)>", such as bt.connect 7C:59:48:2E:A4:51 random
5. Check current LE RX/TX maximum data length and time, press "bt.info", as blow, default RX/TX maximum data length is 27 and default RX/TX maxumum time is 328.
Type: LE, Role: master, Id: 0
7C:59:48:2E:A4:51 (random)
Remote address: 7C:59:48:2E:A4:51 (random) (resolvable)
Local address: C0:95:DA:00:BC:82 (public) (identity)
Remote on-air address: 7C:59:48:2E:A4:51 (random) (resolvable)
Local on-air address: 59:8F:3C:20:93:86 (random) (resolvable)
Interval: 0x0024 (45 ms)
Latency: 0x0000 (0 ms)
Supervision timeout: 0x0190 (4000 ms)
LE PHY: TX PHY LE 1M, RX PHY LE 1M
LE data len: TX (len: 27 time: 328) RX (len: 27 time: 328)
6. Update maximum tx data length, press "bt.data-len-update <tx_max_len> [tx_max_time]", such as bt.data-len-update 50, below information will be printed.
Calculated tx time: 512
7C:59:48:2E:A4:51 (random)
data len update initiated.
LE data len updated: TX (len: 50 time: 512) RX (len: 27 time: 328)
7. When LE data len is updated by the peer device, below information will be printed.
LE data len updated: TX (len: 50 time: 512) RX (len: 65 time: 632)
  • BLE GATT data signing:

GATT peripheral role side,
1. Initialize the Host, press "bt.init",
2. Advertising, press "bt.advertise on",
3. After the connection is established, perform the pairing sequence,
   it could be started from peripheral side by pressing "bt.security <level>", such as "bt.security 2",
4. After the authentication is successfully, disconnect the connection,
   it could be started from peripheral side by pressing "bt.disconnect",
5. Waiting for new connection. After the connection is established (LL enceyption should be disabled),
   add new serivce "gatt.register".

GATT central role side,
1. Initialize the Host, press "bt.init",
2. Scaning advertising packets, press "bt.scan on",
3. A few seconds later, stop the scanning, press "bt.scan off"
4. Select the target board and create a new connection. If the taregt is not listed, repeat steps 2 and 3.
   Then press "bt.connect <address: XX:XX:XX:XX:XX:XX> <type: (public|random)>"
5. After the connection is established, perform the pairing sequence,
   it could be started from central side by pressing "bt.security <level>", such as "bt.security 2",
6. After the authentication is successfully, disconnect the connection,
   it could be started from central side by pressing "bt.disconnect",
7. Repeat the steps 2 and 3. After the connection is established (LL enceyption should be disabled),
   perform the GATT data signing sequence, press "gatt.signed-write <handle> <data> [length] [repeat]",
   such as "gatt.signed-write 22 AA 1"
  • BLE GATT Service Changed Indication:

GATT peripheral role side,
1. Initialize the Host, press "bt.init",
2. Advertising, press "bt.advertise on",
3. After the connection is established. and waiting for the service changed indication is subsribed,
4. Add new serivce, press "gatt.register",
5. Remove the added serivce, press "gatt.unregister".

GATT central role side,
1. Initialize the Host, press "bt.init",
2. Scaning advertising packets, press "bt.scan on",
3. A few seconds later, stop the scanning, press "bt.scan off"
4. Select the target board and create a new connection. If the taregt is not listed, repeat steps 2 and 3.
   Then press "bt.connect <address: XX:XX:XX:XX:XX:XX> <type: (public|random)>"
5. After the connection is established, subscribe the GATT service changed indicator. press "bt.subscribe <CCC handle> <value handle> [ind]",
   such as "gatt.subscribe f e ind".