Hardware requirements
Mini/micro USB cable
Network cable RJ45 standard
i.MX943-EVK board
Personal Computer
Servo-Motor DELTA_ASDA_B3 * 1 INOVANCE_SV680 * 1
Board settings
No special settings are required.
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Power up the servo-motor and connect it to the target board(J26) via an Ethernet Cable.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Write the program to the flash of the target board.
Start the demo and test SOEM performance.