Hardware requirements
Micro USB cable
two IMX95LP4X-EVK boards
J-Link Debug Probe
12V~20V power supply
Personal Computer
Board settings
Connection as below:
MASTER(LPI2C6) connect to SLAVE(LPI2C6)
Pin Name Board Location Pin Name Board Location
SCL J27 pin 3 SCL J27 pin 3
SDA J27 pin 5 SDA J27 pin 5
GND J27 pin 9 GND J27 pin 9
Please note this application can’t support running with Linux BSP!
Prepare the Demo
Connect 12V~20V power supply and J-Link Debug Probe to the board, switch SW4 to power on the board.
Connect a micro USB cable between the host PC and the J31 USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either re-power up your board or launch the debugger in your IDE to begin running the example
Running the demo
When the example runs successfully, the following message is displayed in the terminal:
CMSIS LPI2C board2board interrupt example -- Slave transfer.
Slave received data :
0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7
0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f
End of LPI2C example .