Hardware requirements
Micro USB cable
IMX95LPD5-EVK board
J-Link Debug Probe
12V~20V power supply
Personal Computer
Board settings
Connect J22-3(GPIO_IO03 pad, I2C6_SCL_3V3) and j22-8(GND) to oscilloscope
Please note this application can’t support running with Linux BSP!
Prepare the Demo
Connect 12V~20V power supply and JLink Plus to the board, switch SW4 to power on the board
Connect a micro USB cable between the host PC and the J31 USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either re-power up your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the example runs successfully, the following message is displayed in the terminal: Since no LED connected to the RGPIO. Please use oscilloscope probe to the pin to check the output. The output will toggle periodically.
RGPIO Driver example
The LED is taking turns to shine.