Hardware requirements
Mini/micro USB cable
K32W148-EVK Board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect the micro and mini USB cable between the PC host and the USB ports on the board.
Open a serial terminal on PC for the serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the example runs successfully, the following message is displayed in the terminal:
EDMA memory to memory transfer example begin.
Destination Buffer:
0 0 0 0
EDMA memory to memory transfer example finish.
Destination Buffer:
1 2 3 4