Hardware requirements
Mini/micro USB cable
K32W148-EVK Board
Personal Computer
Board settings
To make the example work, connections needed to be as follows: Jumper setting:
EVK board: ~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~ MASTER(I3C0) connect to SLAVE(I3C0) Pin Name Board Location Pin Name Board Location SCL J2 pin 9 SCL J2 pin 9 SDA J2 pin 10 SDA J2 pin 10 GND J10 pin 4 GND J10 pin 4 ~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
Other jumpers keep default configuration.
Prepare the Demo
Connect the micro and mini USB cable between the PC host and the USB ports on the board.
Open a serial terminal on PC for the serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The following lines are printed to the serial terminal when the demo program is executed.
I3C board2board polling example -- Slave transfer.
Check I3C master I2C transfer.
Slave received data :
0x 1 0x20 0x 0 0x 1 0x 2 0x 3 0x 4 0x 5
0x 6 0x 7 0x 8 0x 9 0x a 0x b 0x c 0x d
0x e 0x f 0x10 0x11 0x12 0x13 0x14 0x15
0x16 0x17 0x18 0x19 0x1a 0x1b 0x1c 0x1d
0x1e 0x1f
I3C master I2C transfer finished.
Check I3C master I3C SDR transfer.
Slave received data :
0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7
0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f
I3C master I3C SDR transfer finished.
Check I3C master I3C HDR transfer.
Slave received data :
0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7
0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f
I3C master I3C HDR transfer finished.