Hardware requirements
Mini/micro USB cable
K32W148-EVK Board
Personal Computer
Board settings
connect input signal to J1-8
Prepare the Demo
Connect a USB cable between the host PC and the EVK board J14.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The following lines are printed to the serial terminal when the demo program is executed.
TPM input capture example
Once the input signal is received the input capture value is printed
Capture value C(n)V=27da02b