Overview
The LIN (Local Interconnect Network) demo application is a use-case of LIN stack driver built on Low Power UART. This application demonstrates a signal transfer between the two nodes. Master node and slave node signals. Both master and slave node must have implemented the timer that is used by timeout service routine every 500 us and master node use the same timer to check for switch of the frame table scheduler every 5 ms, but the real period between frames may larger than 5ms according to the configurations.
User can use the SW3 button to set master node to sleep and SW2 button to wakeup the master node.
Hardware requirements
Two micro USB cables
Two KW45B41Z-EVK boards
Personal Computer
Power adapter 12 V
Three Dupont female-to-female wires
Board settings
Connect J11-1 of the two boards
Connect J11-2 of the two boards
Connect J11-4 of the two boards
Connect 12 V adapter to J9
Short the JP19-1 and JP19-2 with the jumper
Prepare the Demo
Connect a mini/micro USB cable between the PC host and the OpenSDA USB port on the boards.
Open a serial terminal on PC for OpenSDA serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program for master node to the target board.
Running the demo
If communication is succesfull, the master node will print:
LIN master demo start.
LIN master will receive data from slave node, and send control command to slave.
-> LED 2 is ON!
-> LED 3 is ON!
-> LED 2 is ON!
-> LED 3 is ON!
-> LED 2 is ON!