Hardware requirements
Type-C USB cable
KW47-EVK Board
Personal Computer
Board settings
Prepare the Demo
Connect a USB cable between the host PC and the EVK board J14.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
The J12 Pin 1 (ADC0_A6) on EVK board is used to monitor the voltage. The VREFO 1.8v is used as the ADC reference.
Running the demo
The log below shows the output of the demo in the terminal window:
LPADC Temperature Measurement Example
ADC Full Range: 65536
Please press any key to get temperature from the internal temperature sensor.
Current temperature: 22.319
Current temperature: 22.319
Current temperature: 22.319
Current temperature: 22.319
Current temperature: 22.707
Current temperature: 22.707
Current temperature: 22.707
Current temperature: 22.707