Hardware requirements
Micro USB cable
LPC845 Breakout board
Personal Computer
Board settings
PIO0_17 is DAC0 output pin.
Prepare the demo
Connect a micro USB cable between the PC host and the CMSIS DAP USB port on the board.
Open a serial terminal with the following settings:
9600 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The log below shows the output of the DAC interrupt example in the terminal window:
DAC interrupt Example.
Please probe the signal using an oscilloscope.
Probe the signal of PIO0_17 using an oscilloscope.