Hardware requirements
Micro USB cable
LPCXpresso54S018 board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a micro USB cable between the host PC and the LPC-Link USB port (J8) on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
This demo is an external flash XIP demo, CPU will execute the code in external flash:
Build the demo to generate a bin file. Note: If need to generate bin file using MCUXpresso IDE, below steps need to be followed: Set in example Properties->C/C++ Build->Settings->Build steps->Post-build steps->Edit enbable arm-none-eabi-objcopy -v -O binary “&{BuildArtifactFileName}” “&{BuildArtifactFileBaseName}.bin”
This plainload example linked the vector table to 0x10000000, but program to external flash 0x10000000.
Program the bin file to external on board flash via SEGGER J-FLASH Lite(V6.22 or higher):
a. Open SEGGER J-FLASH Lite, select device LPC54S018.
b. Click the ‘Erase Chip’ to erase the extrenal flash.(if can not success, press SW4 button and reset the board, and try to erase again)
c. Select the bin data file, set the ‘.bin/Erase Start’ address to 0x10000000, then click ‘Program Device’ Note: Please use above way to program the binary file built by armgcc tool chain to external flash. For IAR, KEIL, MCUXpresso IDE, you can use the IDE tool to program the external flash.
Press the reset button.
The log below shows in the terminal window:
Power Manager Demo for LPC device.
The "user key" is: SW5
Select an option
1. Sleep mode
2. Deep Sleep mode
3. Deep power down mode
/* Type in '1' into UART terminal */
Entering Sleep [Press the user key to wakeup] ...
/* Press the user key on board */
Pin event occurs
Wakeup.
Select an option
1. Sleep mode
2. Deep Sleep mode
3. Deep power down mode
/* Type in '2' into UART terminal */
Entering Deep Sleep [Press the user key to wakeup] ...
/* Press the user key on board */
Pin event occurs
Wakeup.
Select an option
1. Sleep mode
2. Deep Sleep mode
3. Deep power down mode
/* Type in '3' into UART terminal */
Entering Deep Powerdown [Reset to wakeup] ...
Press any key to confirm to enter the deep sleep mode and wakeup the device by reset.
/* Type in any key into UART terminal */
/* Press the reset key on board. */
Power Manager Demo for LPC device.
The "user key" is: SW5
Select an option
1. Sleep mode
2. Deep Sleep mode
3. Deep power down mode