Hardware requirements

  • Micro USB cable

  • LPCXpresso54S018 board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo

  1. Connect a micro USB cable between the host PC and the LPC-Link USB port (J8) on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the example runs successfully, the following message is displayed in the terminal:

DMA linked transfer example begin.

Destination Buffer:

0   0   0   0   0   0   0   0

DMA linked transfer example finish.

Destination Buffer:

1   2   3   4   11  22  33  44