Hardware requirements
Mini/micro USB cable
LPCXpresso55S16 board
Personal Computer
Board settings
The jumper setting: Default jumpers configuration does not work, you will need to add JP20 and JP21 (JP22 optional for ADC use)
Prepare the Demo
Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J1) on the board
Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Running the demo
After the board is flashed the Tera Term will print message on terminal.
Example output:
GPIO Driver example
The LED is taking turns to shine.
Standard port read: 40290
Masked port read: 40000
Port state: 64001804
Port state: 64001804
Port state: 64001804
Port state: 64001804
...
When press sw1 the LED GREEN will turn to shine