Hardware requirements
Micro USB cable
LPCXpresso55S36 boards
Personal Computer
Board settings
Prepare the Demo
Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J1) on the board
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Launch the debugger in your IDE to begin running the demo.
Running the demo
When the demo runs successfully, the log would be seen on the terminal like:
Configure DMA
Buffer Data before transfer
<data>
Transfer completed
Buffer Data after transfer
<data>
This example shows how DMA can be used with DMIC to transfer data to memory.DMIC audio data can also be seen in g_rxBuffer. Intially this buffer is initialized to zero.