Hardware requirements

  • Mini/micro USB cable

  • LPCXpresso55s69 board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo

Note: MCUXpresso IDE project default debug console is semihost

  1. Connect a micro USB cable between the PC host and the CMSIS DAP USB port (P6) on the board

  2. Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

The log below shows example output of the CTimer simple PWM demo using interrupts in the terminal window:

CTimer example to generate a PWM signal
This example uses interrupts to update the PWM duty cycle

The blue led will adjust brightness automatic.