Hardware requirements

  • Micro USB cable

  • LPCXpresso55s69 board

  • Personal Computer

Board settings

Output signal		Board location
SCT0_OUT2    		P18-11
SCT0_OUT6    		P18-13 

Prepare the Demo

=============== Note: MCUXpresso IDE project default debug console is semihost

  1. Connect a micro USB cable between the host PC and the LPC-Link USB port (P6) on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

The log below shows example output in the terminal window:

SCTimer example to use it in 16-bit mode
The example shows both 16-bit counters running and toggling an output periodically
  • Probe oscilloscope at P18_11(5HZ) and P18_13(2.5HZ) to see output signal.