Hardware requirements
Mini/micro USB cable
LPCXpresso55s69 board
Personal Computer
Board settings
The switch for this examples is S1 on the board (PIO0_5)
Output signal Board location
SCT0_OUT2 P18-11
SCT0_OUT4 P17-11
Prepare the Demo
=============== Note: MCUXpresso IDE project default debug console is semihost
Connect a micro USB cable between the PC host and the CMSIS DAP USB port (P6) on the board
Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The log below shows example output of the SCTimer multi-state demo in the terminal window:
SCTimer example to output edge-aligned PWM signal
When user presses a switch the PWM signal will be seen from Out 2
When user presses the switch again PWM signal on Out 2 will turn off
The PWM signal from Out 4 will remain active all the time
You’ll see PWM signals on P18_11 and P17_11 using an oscilloscope