Hardware requirements
Micro USB cable
LPCXpresso55S69 board
Personal Computer
Board settings
Connect SPI7 pins to SPI2 pins:
Master(SPI7) Slave(SPI2)
Pin Name Board Location Pin Name Board Location
MISO P17 pin 12 MISO P18 pin 6
MOSI P17 pin 10 MOSI P18 pin 10
SCK P17 pin 14 SCK P18 pin 8
SSEL1 P17 pin 1 SSEL0 P17 pin 16
Prepare the Demo
Note: MCUXpresso IDE project default debug console is semihost
Connect a micro USB cable between the PC host and the CMSIS DAP USB port (P6) on the board
Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.