Hardware requirements
Mini/micro USB cable
LPCXpresso55s69 board
Personal Computer
Board settings
The FreeRTOS Message Buffers multicore project does not call for any special hardware configurations. Although not required, the recommendation is to leave the development board jumper settings and configurations in default state when running this demo.
Prepare the Demo
Connect a micro USB cable between the PC host and the CMSIS DAP USB port (P6) on the board
Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
For detailed instructions, see the appropriate board User’s Guide.
Running the demo
The log below shows the output of the FreeRTOS Message Buffers multicore demo in the terminal window:
FreeRTOS Message Buffers demo starts
Copy CORE1 image to address: 0x20033000, size: 15548
Primary core received a msg
Message: Size=4, DATA = 1
Primary core received a msg
Message: Size=4, DATA = 3
Primary core received a msg
Message: Size=4, DATA = 5
.
.
.
Primary core received a msg
Message: Size=4, DATA = 101
FreeRTOS Message Buffers demo ends
Note: The “Copy CORE1 image to address…” log message is not displayed on the terminal window when MCUXpresso IDE is used. In case of MCUXpresso IDE the secondary core image is copied to the target memory during startup automatically.