Hardware requirements

  • Micro USB cable

  • LPCXpresso802 board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo

  1. Connect a micro USB cable between the host PC and the CMSIS DAP port(CN1 on the board).

  2. Open a serial terminal with the following settings:

    • 9600 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

Running the demo

  1. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

The following lines are printed to the serial terminal when the demo program is executed.

IAP Flash example

Writing flash sector 1

Erasing flash sector 1

Erasing page 1 in flash sector 1

Flash signature value of page 1

XXXXXXXXXXXXXXXXXXXXX

End of IAP Flash Example