Hardware Requirements
Mini/micro USB cable
LPCXpresso824MAX board
Personal Computer
Board Settings
Connect SJ9: 2-3
Run the Demo
Connect a micro USB cable between the PC host and the CMSIS DAP port(J3 on the board).
Open a serial terminal with the following settings:
9600 baud rate
8 data bits
No parity
One stop bit
No flow control
Choose an IDE, building the project and download the program to the target board. More information about how to compile and program the project can refer to the
[Getting Started with MCUXpresso SDK](../../../../docs/Getting Started with MCUXpresso SDK.pdf).
Launch the debugger in your IDE to begin running the demo.
Expected Result
Board will print “hello world.” to the terminal, and if users input some characters, board will send them back to the terminal emulator immediately.