Toolchain supported
IAR embedded Workbench 8.11.3
Keil MDK 5.23
MCUXpresso10.1.0
Hardware requirements
Micro USB cable
LPCXpresso824MAX board
Personal Computer
Board settings
ADC CH1 input signal J5-1(PIO0-6).
Prepare the Demo
Connect a micro USB cable between the host PC and the LPC-Link USB port (J3) on the target board.
Open a serial terminal with the following settings:
9600 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The log below shows the output of the hello world demo in the terminal window:
ADC interrupt example.
ADC Calibration Done.
Configuration Done.
ADC Full Range: XXXX
gAdcResultInfoStruct.result = 547
gAdcResultInfoStruct.channelNumber = 1
gAdcResultInfoStruct.overrunFlag = 0
gAdcResultInfoStruct.result = 549
gAdcResultInfoStruct.channelNumber = 1
gAdcResultInfoStruct.overrunFlag = 0
gAdcResultInfoStruct.result = 551
gAdcResultInfoStruct.channelNumber = 1
gAdcResultInfoStruct.overrunFlag = 0
...