Hardware requirements
Mini/micro USB cable
LPCXpresso824MAX board
Personal Computer
Board settings
Connect SJ9: 2-3 Prepare the Demo
Connect a micro USB cable between the PC host and the CMSIS DAP USB port on the board
Open a serial terminal with the following settings:
9600 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The log below shows the output of the hello world demo in the terminal window:
Usart interrupt transfer example.
Board receives 8 characters then sends them out.
Now please input: