ardware requirements

  • Micro USB cable

  • LPCXpresso860MAX board

  • Personal Computer

Board settings

Prepare the Demo

  1. Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J4) on the board

  2. Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):

    • 9600 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the example runs successfully, the following message is displayed in the terminal:

DMA linked transfer example begin.
Destination Buffer:
0	0	0	0	0	0	0	0
DMA linked transfer example finish.
Destination Buffer:
1	2	3	4	11	22	33	44